Qorvo Secures Multiple Mobile Wi-Fi Design Wins

February 23, 2016

BARCELONA, SPAIN – February 23, 2016 – Qorvo® (Nasdaq: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and defense applications, today announced it has secured more than a dozen design wins at leading manufacturers of performance-tier smartphones with its rapidly expanding family of mobile Wi-Fi front end modules. The wins include Qorvo's RF Fusion™ Mobile Wi-Fi iFEM, which delivers a new level of integration and performance in the mobile Wi-Fi front end. Qorvo is uniquely positioned to design and manufacture all of the high-value components in the integrated front end, including high-performance filters, switches, low noise amplifiers, and power amplifiers.

The QM48184 is Qorvo's newest RF Fusion™ Mobile Wi-Fi iFEM. The QM48184 integrates a premium BAW Wi-Fi coexistence filter with 5 GHz and 2.4 GHz power amplifiers, low noise amplifiers, switches, a diplexer, and a coupler, in an extremely compact 4mm x 3mm package. The QM48184 is co-designed and tuned with a global chipset partner to provide superior power output and linearity with low current consumption, helping smartphone manufacturers to maximize data throughput while extending battery life.

The Wi-Fi coexistence filter in the QM48184 leverages Qorvo's proprietary LowDrift™ BAW technology to address the design challenges related to interference between Wi-Fi and the adjacent LTE bands 7, 40 and 41 in China, North America and elsewhere. Qorvo's coexistence filters deliver superior insertion loss to enhance receive sensitivity, power added efficiency (PAE) and power output, helping smartphone manufacturers to extend battery life and maximize data throughput across the full 2.4 GHz Wi-Fi spectrum. All of Qorvo's LowDrift™ and NoDrift™ premium BAW filters combine high performance and temperature stability to solve coexistence challenges unaddressed by other technologies.

The QM48184 employs Qorvo's proprietary wafer-level packaging (WLP) and CuFlip™ flip-chip technology to reduce module size and enable space savings up to 30% versus comparable discrete solutions in 2X2 MIMO configurations.

Qorvo's Wi-Fi portfolio also includes two pairs of FEMs designed for chip-on-board implementations. The RFFM8538 and RFFM8248 provide a complete solution for premium smartphones, including 2X2 MIMO support, while the RFFM8516 and RFFM8216 are optimized for performance-tier smartphones. Each pair consists of a 2.4 GHz module and a complementary 5 GHz module, offering manufacturers the flexibility to implement a dual-band or single-band Wi-Fi solution.

Qorvo's high performance RF solutions simplify design, reduce product footprint, conserve power, improve system performance and accelerate the adoption of carrier aggregation. Qorvo combines deep systems-level expertise, broad manufacturing scale, and the industry's most comprehensive product and technology portfolio to help leading manufacturers accelerate delivery of next-generation LTE, LTE-A, and IoT products. Qorvo's Core RF solutions set the standard for next-gen connectivity, with unmatched integration and performance at the heart of the connected world.

Qorvo is showcasing the Company’s expanding portfolio of high performance RF solutions for smartphones, tablets, and other high-performance mobile data devices at the 2016 GSMA Mobile World Congress, February 22-25, 2016, in Barcelona.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 7,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries.

Investor Relations:
Doug DeLieto
VP, Investor Relations
Qorvo
+1-336-678-7088


Marketing Manager:
Abhiroop Dutta
Strategic Marketing Communications Manager
Qorvo Mobile Products
+1-336-678-8074
abhiroop.dutta@qorvo.com


This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
Qorvo Secures Multiple Mobile Wi-Fi Design Wins

February 23, 2016

BARCELONA, SPAIN – February 23, 2016 – Qorvo® (Nasdaq: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and defense applications, today announced it has secured more than a dozen design wins at leading manufacturers of performance-tier smartphones with its rapidly expanding family of mobile Wi-Fi front end modules. The wins include Qorvo's RF Fusion™ Mobile Wi-Fi iFEM, which delivers a new level of integration and performance in the mobile Wi-Fi front end. Qorvo is uniquely positioned to design and manufacture all of the high-value components in the integrated front end, including high-performance filters, switches, low noise amplifiers, and power amplifiers.

The QM48184 is Qorvo's newest RF Fusion™ Mobile Wi-Fi iFEM. The QM48184 integrates a premium BAW Wi-Fi coexistence filter with 5 GHz and 2.4 GHz power amplifiers, low noise amplifiers, switches, a diplexer, and a coupler, in an extremely compact 4mm x 3mm package. The QM48184 is co-designed and tuned with a global chipset partner to provide superior power output and linearity with low current consumption, helping smartphone manufacturers to maximize data throughput while extending battery life.

The Wi-Fi coexistence filter in the QM48184 leverages Qorvo's proprietary LowDrift™ BAW technology to address the design challenges related to interference between Wi-Fi and the adjacent LTE bands 7, 40 and 41 in China, North America and elsewhere. Qorvo's coexistence filters deliver superior insertion loss to enhance receive sensitivity, power added efficiency (PAE) and power output, helping smartphone manufacturers to extend battery life and maximize data throughput across the full 2.4 GHz Wi-Fi spectrum. All of Qorvo's LowDrift™ and NoDrift™ premium BAW filters combine high performance and temperature stability to solve coexistence challenges unaddressed by other technologies.

The QM48184 employs Qorvo's proprietary wafer-level packaging (WLP) and CuFlip™ flip-chip technology to reduce module size and enable space savings up to 30% versus comparable discrete solutions in 2X2 MIMO configurations.

Qorvo's Wi-Fi portfolio also includes two pairs of FEMs designed for chip-on-board implementations. The RFFM8538 and RFFM8248 provide a complete solution for premium smartphones, including 2X2 MIMO support, while the RFFM8516 and RFFM8216 are optimized for performance-tier smartphones. Each pair consists of a 2.4 GHz module and a complementary 5 GHz module, offering manufacturers the flexibility to implement a dual-band or single-band Wi-Fi solution.

Qorvo's high performance RF solutions simplify design, reduce product footprint, conserve power, improve system performance and accelerate the adoption of carrier aggregation. Qorvo combines deep systems-level expertise, broad manufacturing scale, and the industry's most comprehensive product and technology portfolio to help leading manufacturers accelerate delivery of next-generation LTE, LTE-A, and IoT products. Qorvo's Core RF solutions set the standard for next-gen connectivity, with unmatched integration and performance at the heart of the connected world.

Qorvo is showcasing the Company’s expanding portfolio of high performance RF solutions for smartphones, tablets, and other high-performance mobile data devices at the 2016 GSMA Mobile World Congress, February 22-25, 2016, in Barcelona.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 7,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries.

Investor Relations:
Doug DeLieto
VP, Investor Relations
Qorvo
+1-336-678-7088


Marketing Manager:
Abhiroop Dutta
Strategic Marketing Communications Manager
Qorvo Mobile Products
+1-336-678-8074
abhiroop.dutta@qorvo.com


This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.