PAC25xxx Example Code v1.0

This release adds support for the PAC25140 device.
For more detailed version history, see .\pac25xxx_peripheral_examples\project_version.h

Make sure to download the appropriate PAC55xx support package for the desired IDE
using a myActive login from the following link:
https://www.qorvo.com/products/p/PAC5532A#evaluation-tools


IAR, Keil, and Eclipse IDE projects are provided in the example code.


The pac25xxx_peripheral_examples contains example code for the majority of the PAC25140 device peripherals.