DecaWave [Now Qorvo] Launches Industry's Most Precise Indoor Location and Communication CMOS Chip

November 8, 2013
Provides +/-10cm precision with ultra-low power, enabling new RTLS applications

DUBLIN, IRELAND – November 7, 2013 – Fabless semiconductor company DecaWave announced today its first single chip of the ScenSor wireless technology family DW1000, which makes indoor location and communications more accurate, cost-effective and power-efficient than ever before. This is the first Integrated Circuit on the market to electronically identify the specific distance to any object, person or thing with +/-10cm precision.

With multiple patents, DecaWave's ScenSor works by transmitting wireless signals to readers that use them to locate the tagged object to within 10cm. The chip is the smallest device of its class, is compliant with IEEE 802.15.4a standards (now IEEE802.15.4-2011), and uses ultra-low power – it can operate several years from a battery cell or within an energy harvesting environment. These features make the chip functionally and economically viable to deploy, both in volume and in remote locations.

ScenSor can either replace or complement the Radio Frequency Identification (RFID) and WiFi technology currently used for indoor tracking (where GPS signals are unavailable) by allowing for more specific, minute-to-minute location information for high-value goods over short range and through obstructions providing more accuracy than ever before. This brings new opportunities across multiple industries including future applications for the technology incorporated in smartphones and tablets.

Supporting Quotes

Daniel Aljadef, VP Emerging Technologies & IP at Stanley Healthcare (AeroScout):

"The ScenSor chip commences a new era in the world of UWB RTLS by providing excellent performance along with a flexible architecture and very rich functionality. I believe that the ScenSor chip will empower new solutions for many of the most demanding RTLS applications."

Serge Hethuin, Head of secured wireless products (SWP) at THALES Communications & Security (TCS):

"TCS has for many years been developing equipment and devices using UWB. TCS has compared the different waveforms that could be qualified has such. It became obvious that the solution proposed by DecaWave was the best suited one in order to satisfy the demanding applications under consideration. TCS has monitored DecaWave's IC development progress over time, giving evaluation feedback and highlighting application requirements and needs. And today the performance of the DecaWave IC is exceptional and undisputable. TCS focus applications are related to indoor location in urgency situations dealing with different environment types and especially those in severe non line-of-sight conditions, for which multipath fading is a primary concern. The results achieved with the DecaWave IC are particularly good."

Dr. Rae Pu, CEO, DR2 Technologies:

"DecaWave's industry leadership and RTLS expertise has enabled DR2 Technologies to provide indoor positioning systems with peerless flexibility and resolution. We are grateful for their dedicated engineering team and ongoing partnership."

Ciaran Connell, CEO at DecaWave:

"Until now, 10cm location communications across close distances was not possible and current systems with meter-level accuracy have limited reliability, signals would be lost and there was a high risk for error. Customers ask for more than average accuracy most of the time. Our new ScenSor chip changes all that, it provides unprecedented accuracy all the time. More than 1,800 firms and institutes have expressed interest in implementing our technology for applications such as factory and building automation, agriculture, healthcare, ePOS and retail, and warehousing. We've created a foundation for all locator systems, and the systems can now be tailored to specific applications and environments."

About DecaWave

DecaWave is a pioneering fabless semiconductor company developing a family of integrated circuit products called ScenSor, compliant to the IEEE802.15.4a standard, which can electrically identify the specific location of any object, person or thing in an indoor environment at very competitive cost, ultra-low power and with a required level of precision never achieved before +/-10cm. With applications in diverse markets including factory and building automation, agriculture, healthcare, ePOS and retail, and warehousing, the company's flagship DW1000 chip has garnered interest from more than 1,800 firms, research centers and individuals. DecaWave is headquartered in Dublin Ireland, with offices in France, South Korea and Taiwan, and will open a US office early next year. www.decawave.com

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
DecaWave [Now Qorvo] Launches Industry's Most Precise Indoor Location and Communication CMOS Chip

November 8, 2013
Provides +/-10cm precision with ultra-low power, enabling new RTLS applications

DUBLIN, IRELAND – November 7, 2013 – Fabless semiconductor company DecaWave announced today its first single chip of the ScenSor wireless technology family DW1000, which makes indoor location and communications more accurate, cost-effective and power-efficient than ever before. This is the first Integrated Circuit on the market to electronically identify the specific distance to any object, person or thing with +/-10cm precision.

With multiple patents, DecaWave's ScenSor works by transmitting wireless signals to readers that use them to locate the tagged object to within 10cm. The chip is the smallest device of its class, is compliant with IEEE 802.15.4a standards (now IEEE802.15.4-2011), and uses ultra-low power – it can operate several years from a battery cell or within an energy harvesting environment. These features make the chip functionally and economically viable to deploy, both in volume and in remote locations.

ScenSor can either replace or complement the Radio Frequency Identification (RFID) and WiFi technology currently used for indoor tracking (where GPS signals are unavailable) by allowing for more specific, minute-to-minute location information for high-value goods over short range and through obstructions providing more accuracy than ever before. This brings new opportunities across multiple industries including future applications for the technology incorporated in smartphones and tablets.

Supporting Quotes

Daniel Aljadef, VP Emerging Technologies & IP at Stanley Healthcare (AeroScout):

"The ScenSor chip commences a new era in the world of UWB RTLS by providing excellent performance along with a flexible architecture and very rich functionality. I believe that the ScenSor chip will empower new solutions for many of the most demanding RTLS applications."

Serge Hethuin, Head of secured wireless products (SWP) at THALES Communications & Security (TCS):

"TCS has for many years been developing equipment and devices using UWB. TCS has compared the different waveforms that could be qualified has such. It became obvious that the solution proposed by DecaWave was the best suited one in order to satisfy the demanding applications under consideration. TCS has monitored DecaWave's IC development progress over time, giving evaluation feedback and highlighting application requirements and needs. And today the performance of the DecaWave IC is exceptional and undisputable. TCS focus applications are related to indoor location in urgency situations dealing with different environment types and especially those in severe non line-of-sight conditions, for which multipath fading is a primary concern. The results achieved with the DecaWave IC are particularly good."

Dr. Rae Pu, CEO, DR2 Technologies:

"DecaWave's industry leadership and RTLS expertise has enabled DR2 Technologies to provide indoor positioning systems with peerless flexibility and resolution. We are grateful for their dedicated engineering team and ongoing partnership."

Ciaran Connell, CEO at DecaWave:

"Until now, 10cm location communications across close distances was not possible and current systems with meter-level accuracy have limited reliability, signals would be lost and there was a high risk for error. Customers ask for more than average accuracy most of the time. Our new ScenSor chip changes all that, it provides unprecedented accuracy all the time. More than 1,800 firms and institutes have expressed interest in implementing our technology for applications such as factory and building automation, agriculture, healthcare, ePOS and retail, and warehousing. We've created a foundation for all locator systems, and the systems can now be tailored to specific applications and environments."

About DecaWave

DecaWave is a pioneering fabless semiconductor company developing a family of integrated circuit products called ScenSor, compliant to the IEEE802.15.4a standard, which can electrically identify the specific location of any object, person or thing in an indoor environment at very competitive cost, ultra-low power and with a required level of precision never achieved before +/-10cm. With applications in diverse markets including factory and building automation, agriculture, healthcare, ePOS and retail, and warehousing, the company's flagship DW1000 chip has garnered interest from more than 1,800 firms, research centers and individuals. DecaWave is headquartered in Dublin Ireland, with offices in France, South Korea and Taiwan, and will open a US office early next year. www.decawave.com

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.