Qorvos New SOI Components Enhance High Performance Broadband Communications Systems

May 20, 2015

High performance components landing major design wins at cellular base station manufacturers

GREENSBORO, N.C. and HILLSBORO, Ore. – May 20, 2015 – Qorvo, Inc. (Nasdaq: QRVO), a leading provider of RF solutions for mobile, infrastructure and aerospace/defense applications, today announced new high-performance Silicon-on-Insulator (SOI) components ideal for broadband communications systems. The highly integrated components significantly reduce external components while lowering cost, power consumption, and weight in wireless infrastructure, test and measurement, and defense and aerospace applications.

"These new SOI components feature the broadband performance our customers expect from Qorvo™'s products," said Sumit Tomar, general manager of Qorvo's Wireless Infrastructure business unit. "With exceptional linearity, robust power handling, and no external components, this portfolio is already in demand, even in the sampling stage."

Qorvo now offers the following RF switches, temperature compensating attenuator (TCA), digital step attenuators (DSA), and a programmable array of capacitors (PAC).

  • The RFSW60x2 family of 5-6,000 MHz multi-throw switches features an industry-leading combination of insertion loss, linearity, and isolation. With three-to-six throws, it comes in a tiny 2x2 mm QFN package. Qorvo also launched a high isolation (60 dB) SOI switch, RFSW6024, which is landing major design wins at cellular base station manufacturers. These broadband switches require no external blocking capacitors.
  • The RFSA4033 is a new 5-6,000 MHz analog TCA that features exceptional linearity over its entire gain control range. This TCA offsets the gain reduction of an RF lineup over temperature without the need for closed loop feedback. Eight selectable scaled attenuation slopes and eight selectable attenuation values at 25°C create a total combination of 64 possible temperature coefficients, making it a flexible solution for RF lineups.
  • Several new 5-6000MHz high-performance DSAs, RFSA3xxx, are available with four- to seven-bit controls and a novel overshoot-free switching architecture. This design eliminates troublesome transient glitches when switching between attenuation states. These DSAs allow up to eight devices to operate from a single controller.
  • The RFAC3612, a 6-bit, 64-state PAC for tunable RF applications offers high-power handling, high Q and excellent linearity, making it an ideal component for tunable RF phase shifters, filters, amplifier matching networks and antenna-tuning networks. The RFAC3612 is packaged in a tiny 2x2.5mm, 10-pin package.

 

These components also feature ESD protection and low DC power, ideal for broadband high-performance communications systems. Production samples are available immediately through local Qorvo sales channels.

Qorvo is exhibiting at Booth 331 at the IEEE International Microwave Symposium (IMS), May 18-21 in Phoenix, Arizona. Discuss these new products and more with us at the show or online using #IMS2015 and #QorvoIMS.

About Qorvo

Qorvo (Nasdaq:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 6,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com


This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
Qorvos New SOI Components Enhance High Performance Broadband Communications Systems

May 20, 2015

High performance components landing major design wins at cellular base station manufacturers

GREENSBORO, N.C. and HILLSBORO, Ore. – May 20, 2015 – Qorvo, Inc. (Nasdaq: QRVO), a leading provider of RF solutions for mobile, infrastructure and aerospace/defense applications, today announced new high-performance Silicon-on-Insulator (SOI) components ideal for broadband communications systems. The highly integrated components significantly reduce external components while lowering cost, power consumption, and weight in wireless infrastructure, test and measurement, and defense and aerospace applications.

"These new SOI components feature the broadband performance our customers expect from Qorvo™'s products," said Sumit Tomar, general manager of Qorvo's Wireless Infrastructure business unit. "With exceptional linearity, robust power handling, and no external components, this portfolio is already in demand, even in the sampling stage."

Qorvo now offers the following RF switches, temperature compensating attenuator (TCA), digital step attenuators (DSA), and a programmable array of capacitors (PAC).

  • The RFSW60x2 family of 5-6,000 MHz multi-throw switches features an industry-leading combination of insertion loss, linearity, and isolation. With three-to-six throws, it comes in a tiny 2x2 mm QFN package. Qorvo also launched a high isolation (60 dB) SOI switch, RFSW6024, which is landing major design wins at cellular base station manufacturers. These broadband switches require no external blocking capacitors.
  • The RFSA4033 is a new 5-6,000 MHz analog TCA that features exceptional linearity over its entire gain control range. This TCA offsets the gain reduction of an RF lineup over temperature without the need for closed loop feedback. Eight selectable scaled attenuation slopes and eight selectable attenuation values at 25°C create a total combination of 64 possible temperature coefficients, making it a flexible solution for RF lineups.
  • Several new 5-6000MHz high-performance DSAs, RFSA3xxx, are available with four- to seven-bit controls and a novel overshoot-free switching architecture. This design eliminates troublesome transient glitches when switching between attenuation states. These DSAs allow up to eight devices to operate from a single controller.
  • The RFAC3612, a 6-bit, 64-state PAC for tunable RF applications offers high-power handling, high Q and excellent linearity, making it an ideal component for tunable RF phase shifters, filters, amplifier matching networks and antenna-tuning networks. The RFAC3612 is packaged in a tiny 2x2.5mm, 10-pin package.

 

These components also feature ESD protection and low DC power, ideal for broadband high-performance communications systems. Production samples are available immediately through local Qorvo sales channels.

Qorvo is exhibiting at Booth 331 at the IEEE International Microwave Symposium (IMS), May 18-21 in Phoenix, Arizona. Discuss these new products and more with us at the show or online using #IMS2015 and #QorvoIMS.

About Qorvo

Qorvo (Nasdaq:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 6,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com


This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.