Qorvo® Launches Compact GaN Power Amplifiers for Advanced Radar Systems

September 30, 2016

L-Band and S-Band PAs significantly improve performance while reducing system costs

GREENSBORO, NC – September 30, 2016 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative RF solutions that connect the world, today introduced two new power amplifiers (PAs) including the industry's first 500-watt, L-Band PA internally matched to 50 ohms. These high-power devices are optimized for use in defense and civilian radar systems, with features designed to shorten and simplify system implementation.

Built on Qorvo's high-performance gallium nitride (GaN) technology, the new QPD1003 meets the performance needs of high-power phased arrays such as Active Electronic Scanned Array (AESA) radars, which operate in the 1.2 to 1.4 GHz frequency range. These systems require PAs that operate at maximum efficiency resulting in low heat generation in demanding environmental conditions. The new QPD1003 addresses these requirements through the innovative use of highly efficient GaN on silicon carbide (SiC) technology.

Roger Hall, general manager of High Performance Solutions at Qorvo said, "This is the first and only compact, internally matched and high-powered L-Band PA for AESA radar. It's a breakthrough technology that will provide substantial cost benefits and performance enhancements for customers."

In addition to the QPD1003 L-Band PA, Qorvo also introduced a 450-watt S-Band PA, designed for 3.1 to 3.5 GHz S-Band radar systems. Both devices offer advantages in size and ease of implementation over conventional GaN transistors. They enable multiple frequency bands to be covered by a single matched design, which reduces circuit footprint and overall complexity when used in multi-kilowatt arrays. Additionally, reducing the amount of power dissipation results in further system operational savings by reducing the need to cool the system.

The new PAs support pulsed and linear operations, and are supplied in an air cavity package suited for defense and civilian radar applications. The table below outlines specifications for each.

Product Freq (GHz) Vd(V) Psat (W) PAE (%) LS Gain (dB)
QPD1003 1.2-1.4 50 500 62 17
QPD1017 3.1-3.5 50 450 57 13

Additional information about Qorvo's solutions for mission-critical applications can be found here: www.qorvo.com/defense.

Qorvo is the leading GaN RF supplier for the defense and cable industries*. Since 1999, Qorvo has been driving GaN research and innovation, offering proven GaN circuit reliability and compact, highly efficient products. Qorvo is a Defense Manufacturing Electronics Agency accredited 1A Trusted Source, having completed the Defense Production Act Title III GaN on SiC program in 2014. The Company remains the only GaN supplier to achieve Manufacturing Readiness Level (MRL) 9. Qorvo drives the innovation of GaN products for next-generation systems – from DC through Ka-band – that offer robust performance, low maintenance and long operational lifetimes.

*Strategy Analytics 2016

About Qorvo

Qorvo (NASDAQ:QRVO) makes a better world possible by providing innovative RF solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage our unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries.

Investor Relations Contact:
Doug DeLieto
VP, Investor Relations
+1-336-678-7088
Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of integrating the businesses of RFMD and TriQuint. These and other risks and uncertainties, which are described in more detail in Qorvo's most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
Qorvo® Launches Compact GaN Power Amplifiers for Advanced Radar Systems

September 30, 2016

L-Band and S-Band PAs significantly improve performance while reducing system costs

GREENSBORO, NC – September 30, 2016 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative RF solutions that connect the world, today introduced two new power amplifiers (PAs) including the industry's first 500-watt, L-Band PA internally matched to 50 ohms. These high-power devices are optimized for use in defense and civilian radar systems, with features designed to shorten and simplify system implementation.

Built on Qorvo's high-performance gallium nitride (GaN) technology, the new QPD1003 meets the performance needs of high-power phased arrays such as Active Electronic Scanned Array (AESA) radars, which operate in the 1.2 to 1.4 GHz frequency range. These systems require PAs that operate at maximum efficiency resulting in low heat generation in demanding environmental conditions. The new QPD1003 addresses these requirements through the innovative use of highly efficient GaN on silicon carbide (SiC) technology.

Roger Hall, general manager of High Performance Solutions at Qorvo said, "This is the first and only compact, internally matched and high-powered L-Band PA for AESA radar. It's a breakthrough technology that will provide substantial cost benefits and performance enhancements for customers."

In addition to the QPD1003 L-Band PA, Qorvo also introduced a 450-watt S-Band PA, designed for 3.1 to 3.5 GHz S-Band radar systems. Both devices offer advantages in size and ease of implementation over conventional GaN transistors. They enable multiple frequency bands to be covered by a single matched design, which reduces circuit footprint and overall complexity when used in multi-kilowatt arrays. Additionally, reducing the amount of power dissipation results in further system operational savings by reducing the need to cool the system.

The new PAs support pulsed and linear operations, and are supplied in an air cavity package suited for defense and civilian radar applications. The table below outlines specifications for each.

Product Freq (GHz) Vd(V) Psat (W) PAE (%) LS Gain (dB)
QPD1003 1.2-1.4 50 500 62 17
QPD1017 3.1-3.5 50 450 57 13

Additional information about Qorvo's solutions for mission-critical applications can be found here: www.qorvo.com/defense.

Qorvo is the leading GaN RF supplier for the defense and cable industries*. Since 1999, Qorvo has been driving GaN research and innovation, offering proven GaN circuit reliability and compact, highly efficient products. Qorvo is a Defense Manufacturing Electronics Agency accredited 1A Trusted Source, having completed the Defense Production Act Title III GaN on SiC program in 2014. The Company remains the only GaN supplier to achieve Manufacturing Readiness Level (MRL) 9. Qorvo drives the innovation of GaN products for next-generation systems – from DC through Ka-band – that offer robust performance, low maintenance and long operational lifetimes.

*Strategy Analytics 2016

About Qorvo

Qorvo (NASDAQ:QRVO) makes a better world possible by providing innovative RF solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage our unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries.

Investor Relations Contact:
Doug DeLieto
VP, Investor Relations
+1-336-678-7088
Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of integrating the businesses of RFMD and TriQuint. These and other risks and uncertainties, which are described in more detail in Qorvo's most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.