Qorvo® Launches Newest Generation of Multi-Time Programmable Power Management ICs

December 7, 2020

Built-in configurability speeds time to market for solid-state drives, video, router, mobile and IoT devices

CMD328K3

GREENSBORO, NC – December 7, 2020 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative solutions that connect and power the world, today introduced a new multi-time programmable family of power management ICs (PMICs) optimized for high performance and compact form-factor designs.

The Qorvo ACT88327/8/9/1 Constant-On-Time (COT) PMIC family accelerates time to market by delivering design flexibility for multiple applications, from SSD cards, computer vision – such as security cameras – and routers to low-power mobile uses (LPDDR5), home control and voice assisted devices. The same base part can be used to support different end products simply by changing the PMIC configuration without special software or firmware. Manufacturers can debug their design and change settings in real time without changing external components.

The new PMICs integrate five voltage rails, a sequencer and seven configurable General Purpose IOs (GPIOs) in a very small, 2.18 x 2.58 mm 30-ball WLCSP package. Each PMIC includes three DC/DC step down converters using integrated power FETs and two low-dropout regulators (LDOs). All are highly configurable via the I2C interface. Other configurations include:

  • Buck1 and LDO1 can be configured as a load switch
  • Buck1 is a peak current mode, fixed frequency DC-DC step down converter that is optimized for output voltage closest to the input voltage
  • Buck1 switches at either 1.125 MHz or 2.25 MHz, requiring only three small components for operation
  • Buck2 and Buck3 use an asynchronous constant on-time, ACOT, control architecture to optimize the load transient response with smaller output capacitors
  • All Bucks work with 0.47uH inductor and require only three small components for operation
  • LDO1 can support up to 390mA and 1A current in bypass mode
  • Both LDOs require only small ceramic capacitors

 

The ACT88329 is the first integrated PMIC in this configuration to support output voltage as low as 0.5V for low output applications like LPDDR5.

The ACT88327/8/9/1 PMIC family has multiple GPIOs that can be configured for different features and purposes like interrupt, reset, external enable, external PG, regulator ON/OFF, DVS, VID, sleep/deep sleep modes, power recycle, and push button. In addition, they support two-level input voltage monitoring. Other examples of configurable options in the PMIC family include startup time, slew rate, system-level sequencing, switching frequency, sleep modes and operating modes. The proprietary ACOT control mode gives the best performance at low output voltage.

David Briggs, senior director of Qorvo's Programmable Power Management business, said, "Qorvo continues to push the limits of integration and configurability in small form-factor PMICs with multi-time programmability. This enables our customers to bring new products to market faster by shortening design cycle time."

The ACT88327 and ACT88329 are available now. Additional product details can be found at www.qorvo.com. Qorvo's Programmable Power Management business delivers power management and intelligent motor drive expertise to key growth markets. The company’s portfolio of analog and mixed-signal SoCs provides scalable core platforms used in charging, powering and embedded digital control systems for industrial, commercial and consumer applications. Qorvo offers Power Application Controllers® (PAC™) and DC-DC power management products that significantly improve system reliability while reducing solution size, cost and system development time. Learn more at www.qorvo.com/products/power-management.

About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries. All other trademarks are the property of their respective owners.

Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1 972-994-8546
katie.caballero@qorvo.com

This press release includes “forward-looking statements” within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions, and are not historical facts and typically are identified by use of terms such as “may,” “will,” “should,” “could,” “expect,” “plan,” “anticipate,” “believe,” “estimate,” “predict,” “potential,” “continue” and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management’s current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under U.S. federal securities laws. Our business is subject to numerous risks and uncertainties, including those relating to fluctuations in our operating results; our substantial dependence on developing new products and achieving design wins; our dependence on a few large customers for a substantial portion of our revenue; a loss of revenue if contracts with the United States government or defense and aerospace contractors are canceled or delayed or if defense spending is reduced; the COVID-19 pandemic, which has and will likely continue to negatively impact the global economy and disrupt normal business activities, and which may have an adverse effect on our results of operations; our dependence on third parties; risks related to sales through distributors; risks associated with the operation of our manufacturing facilities; business disruptions; poor manufacturing yields; increased inventory risks and costs due to timing of customer forecasts; our inability to effectively manage or maintain evolving relationships with platform providers; risks from international sales and operations; economic regulation in China; changes in government trade policies, including imposition of tariffs and export restrictions; our ability to implement innovative technologies; underutilization of manufacturing facilities as a result of industry overcapacity; we may not be able to borrow funds under our credit facility or secure future financing; we may not be able to generate sufficient cash to service all of our debt; restrictions imposed by the agreements governing our debt; volatility in the price of our common stock; damage to our reputation or brand; fluctuations in the amount and frequency of our stock repurchases; our recent and future acquisitions and other strategic investments could fail to achieve financial or strategic objectives; our ability to attract, retain and motivate key employees; our reliance on our intellectual property portfolio; claims of infringement of third-party intellectual property rights; security breaches and other similar disruptions compromising our information; theft, loss or misuse of personal data by or about our employees, customers or third parties; warranty claims, product recalls and product liability; and risks associated with environmental, health and safety regulations and climate change. Many of the foregoing risks and uncertainties are, and will continue to be, exacerbated by the COVID-19 pandemic and any worsening of the global business and economic environment as a result. These and other risks and uncertainties, which are described in more detail in Qorvo’s most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
Qorvo® Launches Newest Generation of Multi-Time Programmable Power Management ICs

December 7, 2020

Built-in configurability speeds time to market for solid-state drives, video, router, mobile and IoT devices

CMD328K3

GREENSBORO, NC – December 7, 2020 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative solutions that connect and power the world, today introduced a new multi-time programmable family of power management ICs (PMICs) optimized for high performance and compact form-factor designs.

The Qorvo ACT88327/8/9/1 Constant-On-Time (COT) PMIC family accelerates time to market by delivering design flexibility for multiple applications, from SSD cards, computer vision – such as security cameras – and routers to low-power mobile uses (LPDDR5), home control and voice assisted devices. The same base part can be used to support different end products simply by changing the PMIC configuration without special software or firmware. Manufacturers can debug their design and change settings in real time without changing external components.

The new PMICs integrate five voltage rails, a sequencer and seven configurable General Purpose IOs (GPIOs) in a very small, 2.18 x 2.58 mm 30-ball WLCSP package. Each PMIC includes three DC/DC step down converters using integrated power FETs and two low-dropout regulators (LDOs). All are highly configurable via the I2C interface. Other configurations include:

  • Buck1 and LDO1 can be configured as a load switch
  • Buck1 is a peak current mode, fixed frequency DC-DC step down converter that is optimized for output voltage closest to the input voltage
  • Buck1 switches at either 1.125 MHz or 2.25 MHz, requiring only three small components for operation
  • Buck2 and Buck3 use an asynchronous constant on-time, ACOT, control architecture to optimize the load transient response with smaller output capacitors
  • All Bucks work with 0.47uH inductor and require only three small components for operation
  • LDO1 can support up to 390mA and 1A current in bypass mode
  • Both LDOs require only small ceramic capacitors

 

The ACT88329 is the first integrated PMIC in this configuration to support output voltage as low as 0.5V for low output applications like LPDDR5.

The ACT88327/8/9/1 PMIC family has multiple GPIOs that can be configured for different features and purposes like interrupt, reset, external enable, external PG, regulator ON/OFF, DVS, VID, sleep/deep sleep modes, power recycle, and push button. In addition, they support two-level input voltage monitoring. Other examples of configurable options in the PMIC family include startup time, slew rate, system-level sequencing, switching frequency, sleep modes and operating modes. The proprietary ACOT control mode gives the best performance at low output voltage.

David Briggs, senior director of Qorvo's Programmable Power Management business, said, "Qorvo continues to push the limits of integration and configurability in small form-factor PMICs with multi-time programmability. This enables our customers to bring new products to market faster by shortening design cycle time."

The ACT88327 and ACT88329 are available now. Additional product details can be found at www.qorvo.com. Qorvo's Programmable Power Management business delivers power management and intelligent motor drive expertise to key growth markets. The company’s portfolio of analog and mixed-signal SoCs provides scalable core platforms used in charging, powering and embedded digital control systems for industrial, commercial and consumer applications. Qorvo offers Power Application Controllers® (PAC™) and DC-DC power management products that significantly improve system reliability while reducing solution size, cost and system development time. Learn more at www.qorvo.com/products/power-management.

About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries. All other trademarks are the property of their respective owners.

Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1 972-994-8546
katie.caballero@qorvo.com

This press release includes “forward-looking statements” within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions, and are not historical facts and typically are identified by use of terms such as “may,” “will,” “should,” “could,” “expect,” “plan,” “anticipate,” “believe,” “estimate,” “predict,” “potential,” “continue” and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management’s current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under U.S. federal securities laws. Our business is subject to numerous risks and uncertainties, including those relating to fluctuations in our operating results; our substantial dependence on developing new products and achieving design wins; our dependence on a few large customers for a substantial portion of our revenue; a loss of revenue if contracts with the United States government or defense and aerospace contractors are canceled or delayed or if defense spending is reduced; the COVID-19 pandemic, which has and will likely continue to negatively impact the global economy and disrupt normal business activities, and which may have an adverse effect on our results of operations; our dependence on third parties; risks related to sales through distributors; risks associated with the operation of our manufacturing facilities; business disruptions; poor manufacturing yields; increased inventory risks and costs due to timing of customer forecasts; our inability to effectively manage or maintain evolving relationships with platform providers; risks from international sales and operations; economic regulation in China; changes in government trade policies, including imposition of tariffs and export restrictions; our ability to implement innovative technologies; underutilization of manufacturing facilities as a result of industry overcapacity; we may not be able to borrow funds under our credit facility or secure future financing; we may not be able to generate sufficient cash to service all of our debt; restrictions imposed by the agreements governing our debt; volatility in the price of our common stock; damage to our reputation or brand; fluctuations in the amount and frequency of our stock repurchases; our recent and future acquisitions and other strategic investments could fail to achieve financial or strategic objectives; our ability to attract, retain and motivate key employees; our reliance on our intellectual property portfolio; claims of infringement of third-party intellectual property rights; security breaches and other similar disruptions compromising our information; theft, loss or misuse of personal data by or about our employees, customers or third parties; warranty claims, product recalls and product liability; and risks associated with environmental, health and safety regulations and climate change. Many of the foregoing risks and uncertainties are, and will continue to be, exacerbated by the COVID-19 pandemic and any worsening of the global business and economic environment as a result. These and other risks and uncertainties, which are described in more detail in Qorvo’s most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.