Qorvo® Boosts Performance with Powerful New Multi-Time Programmable PMIC

May 17, 2021

Product features built-in configurability, sequencing and 13 voltage rails for mid-power applications

GREENSBORO, NC – May 17, 2021 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative radio frequency solutions that connect the world, has expanded its family of multi-time programmable power management ICs (PMICs) with the launch of the company's first Constant-On-Time (COT) PMIC to feature 13 voltage rails and 25 amps of power across all outputs in a 3.8 x 3.8 mm package. The product’s flexibility, small form factor and low quiescent current (LQC) address power, performance and size challenges in applications such as enterprise solid-state drives (SSDs), virtual reality headsets, security and action cameras, and AI processors.

The Qorvo ACT88760 PMIC accelerates time to market for both enterprise and battery-powered consumer applications by enabling designers to change configurations multiple times without special software or firmware. Industry-leading flexibility is achieved with 13 integrated rails, a sequencer and 10 General Purpose IOs (GPIOs) that can be configured for different features. This innovative PMIC also includes seven DC/DC step down converters using integrated power FETs, and six low-dropout regulators (LDOs). All are highly configurable via the I2C interface. Manufacturers can debug designs and change settings in real time without changing external components.

David Briggs, senior director of Qorvo's Programmable Power Management business, said, "Qorvo continues to advance the level of flexibility available to designers. The ACT88760 PMIC delivers the greatest degree of programmability, power efficiency and capability in a simple, compact design. This empowers our customers to innovate enterprise and consumer electronics with greater functionality and extended battery life."

The ACT88760 is available now and offers these features:

ACT88760
  • Bucks 1 & 2: Can operate in dual-phase mode
  • Bucks 3 & 4: Can operate in dual-phase mode
  • Buck 7: Optimized for high efficiency with low VOUT (<1.0V)
  • LDO 1 & 2: Provide 800mA each, PSRR (> 70dB), with Low IQ (~20µA)
  • LDO 5 & 6: Can be configured as 400mA LDOs or as 1.5 amps Load Switches
  • 4 configurable Levels of AVS / DVS and 3 configurable high switching frequency
  • Over-Temperature Protection (OTP), OCP, OV & UV protection
  • 10 configurable GPIOs to enable features such as: VID, DVS interrupt, reset, external enable, external PG, regulator ON/OFF, sleep/deep sleep modes, power recycle, and push button

Qorvo's Programmable Power Management business unit delivers power management and intelligent motor drive expertise to key growth markets. The company's portfolio of analog and mixed-signal SoCs provides scalable core platforms used in charging, powering and embedded digital control systems for industrial, commercial and consumer applications. Qorvo offers Power Application Controllers® (PAC™) and DC-DC power management products that significantly improve system reliability while reducing solution size, cost and system development time. Learn more at www.qorvo.com/powermanagement.

About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo and ConcurrentConnect are trademarks of Qorvo US, Inc. All other trademarks are the property of their respective owners.

Investor Relations Contact:
Doug DeLieto
VP, Investor Relations
+1-336-678-7968

Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1 972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions, and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under U.S. federal securities laws. Our business is subject to numerous risks and uncertainties, including those relating to fluctuations in our operating results; our substantial dependence on developing new products and achieving design wins; our dependence on a few large customers for a substantial portion of our revenue; a loss of revenue if contracts with the United States government or defense and aerospace contractors are canceled or delayed or if defense spending is reduced; our dependence on third parties; risks related to sales through distributors; risks associated with the operation of our manufacturing facilities; business disruptions resulting from natural disasters, extreme weather conditions and public health issues, including the outbreak of COVID-19; poor manufacturing yields; increased inventory risks and costs due to timing of customer forecasts; our inability to effectively manage or maintain evolving relationships with platform providers; risks from international sales and operations; economic regulation in China; changes in government trade policies, including imposition of tariffs and export restrictions; our ability to implement innovative technologies; underutilization of manufacturing facilities as a result of industry overcapacity; we may not be able to borrow funds under our credit facility or secure future financing; we may not be able to generate sufficient cash to service all of our debt; restrictions imposed by the agreements governing our debt; volatility in the price of our common stock; damage to our reputation or brand; fluctuations in the amount and frequency of our stock repurchases; our recent acquisitions and other strategic investments could fail to achieve financial or strategic objectives; our ability to attract, retain and motivate key employees; our reliance on our intellectual property portfolio; claims of infringement of third-party intellectual property rights; security breaches and other similar disruptions compromising our information; theft, loss or misuse of personal data by or about our employees, customers or third parties; warranty claims, product recalls and product liability; and risks associated with environmental, health and safety regulations and climate change. These and other risks and uncertainties, which are described in more detail in Qorvo's most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
|

+1-833-641-3810

Qorvo® Boosts Performance with Powerful New Multi-Time Programmable PMIC

May 17, 2021

Product features built-in configurability, sequencing and 13 voltage rails for mid-power applications

GREENSBORO, NC – May 17, 2021 – Qorvo® (Nasdaq:QRVO), a leading provider of innovative radio frequency solutions that connect the world, has expanded its family of multi-time programmable power management ICs (PMICs) with the launch of the company's first Constant-On-Time (COT) PMIC to feature 13 voltage rails and 25 amps of power across all outputs in a 3.8 x 3.8 mm package. The product’s flexibility, small form factor and low quiescent current (LQC) address power, performance and size challenges in applications such as enterprise solid-state drives (SSDs), virtual reality headsets, security and action cameras, and AI processors.

The Qorvo ACT88760 PMIC accelerates time to market for both enterprise and battery-powered consumer applications by enabling designers to change configurations multiple times without special software or firmware. Industry-leading flexibility is achieved with 13 integrated rails, a sequencer and 10 General Purpose IOs (GPIOs) that can be configured for different features. This innovative PMIC also includes seven DC/DC step down converters using integrated power FETs, and six low-dropout regulators (LDOs). All are highly configurable via the I2C interface. Manufacturers can debug designs and change settings in real time without changing external components.

David Briggs, senior director of Qorvo's Programmable Power Management business, said, "Qorvo continues to advance the level of flexibility available to designers. The ACT88760 PMIC delivers the greatest degree of programmability, power efficiency and capability in a simple, compact design. This empowers our customers to innovate enterprise and consumer electronics with greater functionality and extended battery life."

The ACT88760 is available now and offers these features:

ACT88760
  • Bucks 1 & 2: Can operate in dual-phase mode
  • Bucks 3 & 4: Can operate in dual-phase mode
  • Buck 7: Optimized for high efficiency with low VOUT (<1.0V)
  • LDO 1 & 2: Provide 800mA each, PSRR (> 70dB), with Low IQ (~20µA)
  • LDO 5 & 6: Can be configured as 400mA LDOs or as 1.5 amps Load Switches
  • 4 configurable Levels of AVS / DVS and 3 configurable high switching frequency
  • Over-Temperature Protection (OTP), OCP, OV & UV protection
  • 10 configurable GPIOs to enable features such as: VID, DVS interrupt, reset, external enable, external PG, regulator ON/OFF, sleep/deep sleep modes, power recycle, and push button

Qorvo's Programmable Power Management business unit delivers power management and intelligent motor drive expertise to key growth markets. The company's portfolio of analog and mixed-signal SoCs provides scalable core platforms used in charging, powering and embedded digital control systems for industrial, commercial and consumer applications. Qorvo offers Power Application Controllers® (PAC™) and DC-DC power management products that significantly improve system reliability while reducing solution size, cost and system development time. Learn more at www.qorvo.com/powermanagement.

About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.

Qorvo and ConcurrentConnect are trademarks of Qorvo US, Inc. All other trademarks are the property of their respective owners.

Investor Relations Contact:
Doug DeLieto
VP, Investor Relations
+1-336-678-7968

Media Contact:
Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1 972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions, and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under U.S. federal securities laws. Our business is subject to numerous risks and uncertainties, including those relating to fluctuations in our operating results; our substantial dependence on developing new products and achieving design wins; our dependence on a few large customers for a substantial portion of our revenue; a loss of revenue if contracts with the United States government or defense and aerospace contractors are canceled or delayed or if defense spending is reduced; our dependence on third parties; risks related to sales through distributors; risks associated with the operation of our manufacturing facilities; business disruptions resulting from natural disasters, extreme weather conditions and public health issues, including the outbreak of COVID-19; poor manufacturing yields; increased inventory risks and costs due to timing of customer forecasts; our inability to effectively manage or maintain evolving relationships with platform providers; risks from international sales and operations; economic regulation in China; changes in government trade policies, including imposition of tariffs and export restrictions; our ability to implement innovative technologies; underutilization of manufacturing facilities as a result of industry overcapacity; we may not be able to borrow funds under our credit facility or secure future financing; we may not be able to generate sufficient cash to service all of our debt; restrictions imposed by the agreements governing our debt; volatility in the price of our common stock; damage to our reputation or brand; fluctuations in the amount and frequency of our stock repurchases; our recent acquisitions and other strategic investments could fail to achieve financial or strategic objectives; our ability to attract, retain and motivate key employees; our reliance on our intellectual property portfolio; claims of infringement of third-party intellectual property rights; security breaches and other similar disruptions compromising our information; theft, loss or misuse of personal data by or about our employees, customers or third parties; warranty claims, product recalls and product liability; and risks associated with environmental, health and safety regulations and climate change. These and other risks and uncertainties, which are described in more detail in Qorvo's most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
|

+1-833-641-3810

Qorvo
  • Products
  • Solutions
  • Design Hub
  • Support
  • About Us
Qorvo
Qorvo
Qorvo
  • Products
  • Solutions
  • Design Hub
  • Support
  • About Us
Qorvo
Qorvo