How Not to Run Hot: Overcoming Thermal Challenges in Wi-Fi Front-End Designs (Part 1)

November 14, 2017

Overcoming Thermal Challenges in Wi-Fi Front-End DesignsThis is the first of a two-part blog series that looks at the design challenges for Wi-Fi front-end designs. Part 2 examines coexistence and interference.

For wireless access points or customer premises equipment (CPE), it can be hard to fully account for thermal management and the parameters affected by it prior to FCC certification. To save yourself the headaches of last-minute changes due to interference, coexistence or RF front-end (RFFE) linearity, be sure to design using component thermal parameters in mind. This blog post explains the biggest thermal challenges facing Wi-Fi front-end designs.
 

Increasing capacity for smart homes

On average, today’s households have 12 clients or Internet of Things (IoT) products communicating with each other, but these numbers will increase in coming years. Intel believes the number of household clients will increase to 50 in 2020, while Gartner predicts 20.4 billion connected things will be used worldwide by 2020.

In today’s wireless homes, communication operators and retailers have typically offered one large wireless router, using raw power to achieve coverage across the entire home. But with the sharp increase of household devices and the IoT, smart homes are pushing the capabilities of the single-router model.

As a result, new application models are evolving. Consumers are finding that placing more routers, or nodes, in the home helps service more clients and data backhaul to the home router/modem. This mesh (or distributed Wi-Fi) network model ensures wireless capability across a home using some techniques that are already present in office headquarters, hospitals and college campuses via enterprise-level systems.

Wireless Indoor Architecture

Related Blog Post: How Distributed Wi-Fi Enables Connected Smart Homes
 

The IoT challenge

It’s no surprise that the RF complexity within the access point increases because of this mesh networking model and as devices integrate more standards and capabilities.

The IoT brings several challenges:

  • The addition of wireless radio needs. Access points today incorporate more than just Wi-Fi — they also support Zigbee, Bluetooth, Bluetooth Low Energy (BLE) and Thread. Operators are also finding ways to reach households who previously didn’t have access. Operator-supported LTE-M (the machine-to-machine version of LTE) is one example finding its way into some Wi-Fi gateways.
  • More users within each home. Homes no longer have only one or two PCs and a few phones. Today, several computers, TVs, smartphones, wearables, security networks, wireless appliances and more all connect to Wi-Fi and the internet.
  • Additional Wi-Fi bands. Units no longer have one 2.4 GHz band and one 5 GHz band. Now there are up to eight individual 2.4 GHz and eight 5 GHz paths. This change gives us the MIMO (multiple input / multiple output) and multiuser MIMO (MU-MIMO) paths within the Wi-Fi access point or node.
  • Shrinking size and expanded functionality. Wi-Fi manufacturers are making Wi-Fi units smaller, sleeker, more decorative and less obtrusive. They’re also making some units all-weather or adding multifunctionality such as night-light capability.

Block diagrams of older vs. new access points highlight just how complex the RFFE design is now.

The Evolution of the Wi-Fi Access Point – RFFE Perspective

 

Running hot

All these changes in the Wi-Fi front-end design increase the number of RF chains, contributing to the overall heat within the access point. This increase in unit temperature also increases the RF tuning challenges, especially when the size of the box is the same or even smaller.

In the Wi-Fi world, one of the most critical design challenges engineers need to address is product temperature. In today’s products, components are subject to average temperatures of 60°C or greater, while sitting in a room temperature environment of 25°C. It’s important to consider this fact early on in a design, to help minimize redesign issues or additional costs.
 

How heat challenges RF front ends to deliver capacity and range

Temperature affects three RFFE components:

  1. Power amplifiers
  2. RF switches and low noise amplifiers (LNAs)
  3. Filters

 
Let’s examine the heat challenges and Wi-Fi design considerations for each category.
 

In the Wi-Fi world, one of the most critical design challenges engineers need to address is product temperature.

#1: How does the power amplifier factor in?

Engineers often balance between linearity, power output and efficiency in each of the RF chains. Using optimized, highly linear power amplifiers or front-end modules (FEMs) optimizes system efficiencies, creating less overall heat. It also reduces processing inefficiencies.

High-Tier Wi-Fi Application (8 antennas - 4x4 MU-MIMO, beamforming)

RF engineers should also consider several Wi-Fi design trends that affect power amplifiers:

  • Use of time division duplexing (TDD). Wi-Fi networks use TDD, which means the PAs are pulsed on and off during operation — alternating transmit and receive functions. This increases PA transients, which attribute to high temperatures.
  • More difficult error vector magnitude (EVM) specifications. EVM is a measure of modulation quality and error performance. In 802.11ac, the EVM specification was -35 dB, but in the next standard of Wi-Fi, 802.11ax, this specification increases to -47 dB — which is more difficult for Wi-Fi component designers to meet. Design engineers must design highly linear FEMs to optimize for EVM, which ultimately helps reduce overall product temperature.
  • Higher modulation schemes. To help achieve higher capacity and data rates, Wi-Fi designs are moving from 256 QAM to 1024 QAM modulation schemes. With 1024 QAM modulation, there are more bits per symbol — 10 bits per symbol versus 8 bits in 256 QAM. However, as the data rate increases, EVM on the RFFE becomes a principal concern. The constellation is so dense in 1024 QAM that the processor must use sophisticated system decoding to distinguish each point. When the processor works harder, the unit device heat increases.
  • How the RFFE performance affects the overall current draw on the system processor. Poor RF front-end performance means the processor will have to work harder to meet overall system requirements. Working the processor more increases system hardware heat.

Modulation Changes in 802.11ax
 

#2: What about the RF switch and low noise amplifier (LNA)?

In the switch, insertion loss can also generate excess heat. When insertion loss increases and signal strength is lowered, the PA works harder to compensate and push higher outputs, which degrades efficiency. And less efficiency means more heat from the device. Using high-linearity, low-loss switches keeps the insertion loss within specifications across the entire band.

Receive throughput is highly dependent on the LNA gain and noise figure. Although the LNA doesn’t contribute significantly to heat generation, the effect of heat on the LNA can drastically affect throughput. Heat degrades the noise figure, and depending on the circuit design and choice of wafer technology, the compensation for this can lead a designer to a specific solution.
 

#3: Finally, the filters

RF filters drift to the left or the right due to changes in temperature, as shown in the following SAW vs. BAW figure. These shifts can cause high insertion loss on the band edges, which could cause a low gain or POUT response from the RFFE. If the filter drifts too much (as shown in the SAW figure), then the PA pushes more power output to compensate for the insertion loss. This increases current and decreases system efficiency.

Using filters with high insertion loss can decrease linearity and increase the RF chain POUT. One big advantage of Qorvo’s LowDrift™ bulk acoustic wave (BAW) filters is their stability over temperature shifts. Diplexers, bandpass filters and coexistence filters that use BAW technology with lower temperature drift help mitigate insertion loss, and lead to good product thermals. 

Read More Design Tips: Resolving Interference in a Crowded Wi-Fi Environment Using BAW Filters
 

Temperature Drift of Filter Technology: SAW vs. BAW

Chalk Talk on Wireless Connectivity Front End Solutions

Watch this detailed "Chalk Talk" video to learn more about Qorvo's Wi-Fi connectivity solutions (37:56).

Design considerations for power consumption: Qorvo’s approach

Heat can degrade overall system performance (such as throughput, range and interference resolution). As a result, it’s important to design systems by choosing RFFE components that mitigate the heat. In the transmit chain, the focus should be on balancing link budget needs such as system linear power.

As devices move from 802.11ac to 802.11ax capability, product manufacturers must focus on using more efficient components. Qorvo challenges its design teams to increase linear power without increasing power dissipation — designing higher throughput devices with the same power consumption as previous generations. One example is the QPF4528, an 802.11ax 5 GHz FEM that transmits linear powers achieving -47 dB EVM — above the current QPF4538 FEM, an 802.11ac 5 GHz FEM that achieves ‑43 dB EVM with the lower maximum power dissipation.

Another product that integrates all the aspects of heat mitigation is Qorvo’s QPF7200, a fully integrated front-end module (iFEM) that reduces weight and design complexity while also decreasing system heat. The QPF7200 module:

  • Contains a highly efficient 2 GHz power amplifier to reduce heat
  • Integrates an FCC bandedge LowDrift BAW filter, which is resistant to temperature shifts and provides the option to remove the number of required RF chains
  • Includes an LTE Wi-Fi coexistence filter that negates the interference effects of LTE devices such as phones or modems, which could degrade throughput

QPF7200

QPF7200: iFEM for Access Points

 

Think about operating temperatures before FCC certification

With so many radios and RF chains squeezed together, it’s important to partner with an RF supplier that helps you achieve low power dissipation and linear power budgets simultaneously.

Although many systems are designed and modeled at room temperature, ask yourself how it will operate at 60-70°C (140-158°F) when the device is operating. Don’t wait until FCC certification time to find out.

 

Check out Part 2 in our series, where we address Wi-Fi design challenges around wireless interference/coexistence, and smart tips to overcome them.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
|

+1-833-641-3810

How Not to Run Hot: Overcoming Thermal Challenges in Wi-Fi Front-End Designs (Part 1)

November 14, 2017

Overcoming Thermal Challenges in Wi-Fi Front-End DesignsThis is the first of a two-part blog series that looks at the design challenges for Wi-Fi front-end designs. Part 2 examines coexistence and interference.

For wireless access points or customer premises equipment (CPE), it can be hard to fully account for thermal management and the parameters affected by it prior to FCC certification. To save yourself the headaches of last-minute changes due to interference, coexistence or RF front-end (RFFE) linearity, be sure to design using component thermal parameters in mind. This blog post explains the biggest thermal challenges facing Wi-Fi front-end designs.
 

Increasing capacity for smart homes

On average, today’s households have 12 clients or Internet of Things (IoT) products communicating with each other, but these numbers will increase in coming years. Intel believes the number of household clients will increase to 50 in 2020, while Gartner predicts 20.4 billion connected things will be used worldwide by 2020.

In today’s wireless homes, communication operators and retailers have typically offered one large wireless router, using raw power to achieve coverage across the entire home. But with the sharp increase of household devices and the IoT, smart homes are pushing the capabilities of the single-router model.

As a result, new application models are evolving. Consumers are finding that placing more routers, or nodes, in the home helps service more clients and data backhaul to the home router/modem. This mesh (or distributed Wi-Fi) network model ensures wireless capability across a home using some techniques that are already present in office headquarters, hospitals and college campuses via enterprise-level systems.

Wireless Indoor Architecture

Related Blog Post: How Distributed Wi-Fi Enables Connected Smart Homes
 

The IoT challenge

It’s no surprise that the RF complexity within the access point increases because of this mesh networking model and as devices integrate more standards and capabilities.

The IoT brings several challenges:

  • The addition of wireless radio needs. Access points today incorporate more than just Wi-Fi — they also support Zigbee, Bluetooth, Bluetooth Low Energy (BLE) and Thread. Operators are also finding ways to reach households who previously didn’t have access. Operator-supported LTE-M (the machine-to-machine version of LTE) is one example finding its way into some Wi-Fi gateways.
  • More users within each home. Homes no longer have only one or two PCs and a few phones. Today, several computers, TVs, smartphones, wearables, security networks, wireless appliances and more all connect to Wi-Fi and the internet.
  • Additional Wi-Fi bands. Units no longer have one 2.4 GHz band and one 5 GHz band. Now there are up to eight individual 2.4 GHz and eight 5 GHz paths. This change gives us the MIMO (multiple input / multiple output) and multiuser MIMO (MU-MIMO) paths within the Wi-Fi access point or node.
  • Shrinking size and expanded functionality. Wi-Fi manufacturers are making Wi-Fi units smaller, sleeker, more decorative and less obtrusive. They’re also making some units all-weather or adding multifunctionality such as night-light capability.

Block diagrams of older vs. new access points highlight just how complex the RFFE design is now.

The Evolution of the Wi-Fi Access Point – RFFE Perspective

 

Running hot

All these changes in the Wi-Fi front-end design increase the number of RF chains, contributing to the overall heat within the access point. This increase in unit temperature also increases the RF tuning challenges, especially when the size of the box is the same or even smaller.

In the Wi-Fi world, one of the most critical design challenges engineers need to address is product temperature. In today’s products, components are subject to average temperatures of 60°C or greater, while sitting in a room temperature environment of 25°C. It’s important to consider this fact early on in a design, to help minimize redesign issues or additional costs.
 

How heat challenges RF front ends to deliver capacity and range

Temperature affects three RFFE components:

  1. Power amplifiers
  2. RF switches and low noise amplifiers (LNAs)
  3. Filters

 
Let’s examine the heat challenges and Wi-Fi design considerations for each category.
 

In the Wi-Fi world, one of the most critical design challenges engineers need to address is product temperature.

#1: How does the power amplifier factor in?

Engineers often balance between linearity, power output and efficiency in each of the RF chains. Using optimized, highly linear power amplifiers or front-end modules (FEMs) optimizes system efficiencies, creating less overall heat. It also reduces processing inefficiencies.

High-Tier Wi-Fi Application (8 antennas - 4x4 MU-MIMO, beamforming)

RF engineers should also consider several Wi-Fi design trends that affect power amplifiers:

  • Use of time division duplexing (TDD). Wi-Fi networks use TDD, which means the PAs are pulsed on and off during operation — alternating transmit and receive functions. This increases PA transients, which attribute to high temperatures.
  • More difficult error vector magnitude (EVM) specifications. EVM is a measure of modulation quality and error performance. In 802.11ac, the EVM specification was -35 dB, but in the next standard of Wi-Fi, 802.11ax, this specification increases to -47 dB — which is more difficult for Wi-Fi component designers to meet. Design engineers must design highly linear FEMs to optimize for EVM, which ultimately helps reduce overall product temperature.
  • Higher modulation schemes. To help achieve higher capacity and data rates, Wi-Fi designs are moving from 256 QAM to 1024 QAM modulation schemes. With 1024 QAM modulation, there are more bits per symbol — 10 bits per symbol versus 8 bits in 256 QAM. However, as the data rate increases, EVM on the RFFE becomes a principal concern. The constellation is so dense in 1024 QAM that the processor must use sophisticated system decoding to distinguish each point. When the processor works harder, the unit device heat increases.
  • How the RFFE performance affects the overall current draw on the system processor. Poor RF front-end performance means the processor will have to work harder to meet overall system requirements. Working the processor more increases system hardware heat.

Modulation Changes in 802.11ax
 

#2: What about the RF switch and low noise amplifier (LNA)?

In the switch, insertion loss can also generate excess heat. When insertion loss increases and signal strength is lowered, the PA works harder to compensate and push higher outputs, which degrades efficiency. And less efficiency means more heat from the device. Using high-linearity, low-loss switches keeps the insertion loss within specifications across the entire band.

Receive throughput is highly dependent on the LNA gain and noise figure. Although the LNA doesn’t contribute significantly to heat generation, the effect of heat on the LNA can drastically affect throughput. Heat degrades the noise figure, and depending on the circuit design and choice of wafer technology, the compensation for this can lead a designer to a specific solution.
 

#3: Finally, the filters

RF filters drift to the left or the right due to changes in temperature, as shown in the following SAW vs. BAW figure. These shifts can cause high insertion loss on the band edges, which could cause a low gain or POUT response from the RFFE. If the filter drifts too much (as shown in the SAW figure), then the PA pushes more power output to compensate for the insertion loss. This increases current and decreases system efficiency.

Using filters with high insertion loss can decrease linearity and increase the RF chain POUT. One big advantage of Qorvo’s LowDrift™ bulk acoustic wave (BAW) filters is their stability over temperature shifts. Diplexers, bandpass filters and coexistence filters that use BAW technology with lower temperature drift help mitigate insertion loss, and lead to good product thermals. 

Read More Design Tips: Resolving Interference in a Crowded Wi-Fi Environment Using BAW Filters
 

Temperature Drift of Filter Technology: SAW vs. BAW

Chalk Talk on Wireless Connectivity Front End Solutions

Watch this detailed "Chalk Talk" video to learn more about Qorvo's Wi-Fi connectivity solutions (37:56).

Design considerations for power consumption: Qorvo’s approach

Heat can degrade overall system performance (such as throughput, range and interference resolution). As a result, it’s important to design systems by choosing RFFE components that mitigate the heat. In the transmit chain, the focus should be on balancing link budget needs such as system linear power.

As devices move from 802.11ac to 802.11ax capability, product manufacturers must focus on using more efficient components. Qorvo challenges its design teams to increase linear power without increasing power dissipation — designing higher throughput devices with the same power consumption as previous generations. One example is the QPF4528, an 802.11ax 5 GHz FEM that transmits linear powers achieving -47 dB EVM — above the current QPF4538 FEM, an 802.11ac 5 GHz FEM that achieves ‑43 dB EVM with the lower maximum power dissipation.

Another product that integrates all the aspects of heat mitigation is Qorvo’s QPF7200, a fully integrated front-end module (iFEM) that reduces weight and design complexity while also decreasing system heat. The QPF7200 module:

  • Contains a highly efficient 2 GHz power amplifier to reduce heat
  • Integrates an FCC bandedge LowDrift BAW filter, which is resistant to temperature shifts and provides the option to remove the number of required RF chains
  • Includes an LTE Wi-Fi coexistence filter that negates the interference effects of LTE devices such as phones or modems, which could degrade throughput

QPF7200

QPF7200: iFEM for Access Points

 

Think about operating temperatures before FCC certification

With so many radios and RF chains squeezed together, it’s important to partner with an RF supplier that helps you achieve low power dissipation and linear power budgets simultaneously.

Although many systems are designed and modeled at room temperature, ask yourself how it will operate at 60-70°C (140-158°F) when the device is operating. Don’t wait until FCC certification time to find out.

 

Check out Part 2 in our series, where we address Wi-Fi design challenges around wireless interference/coexistence, and smart tips to overcome them.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
|

+1-833-641-3810

Qorvo
  • Products
  • Solutions
  • Design Hub
  • Support
  • About Us
Qorvo
Qorvo
Qorvo
  • Products
  • Solutions
  • Design Hub
  • Support
  • About Us
Qorvo
Qorvo