Headquarters: Ireland
Region(s) Served: APAC, EMEA, Latin America, North America
Danalto is a technology company specializing in high-accuracy location solutions for complex indoor environments. Their flagship offering, FiLo, leverages a combination of cutting-edge radio technologies—including UWB (Ultra-Wideband), GNSS (Global Navigation Satellite System), Bluetooth, and Wi-Fi—and AI-driven software automation to provide self-deployable, adaptable indoor positioning systems.
FiLo addresses the long-standing challenge of maintaining reliable indoor positioning in dynamic environments where physical changes can disrupt signal accuracy. Instead of requiring manual and costly re-surveying, FiLo enables automated calibration and mesh network formation using both powered and unpowered anchor nodes. These can be installed incrementally, allowing for room-by-room or floor-by-floor deployment, and even convert existing Wi-Fi access points into positioning anchors via USB-enabled sticks.
Danalto’s Cardinal platform is the cloud-based backbone that supports FiLo. It ingests large volumes of real-time IoT and location data, transforming it into actionable insights through analytics, heatmaps, spaghetti diagrams, geo-zoned timelines, and customizable reports. It integrates seamlessly into business workflows via APIs and supports large-scale deployments with robust security and user management.
Designed for industries such as retail, healthcare, logistics, and security, Danalto’s solutions enable real-time tracking of assets and people, enhancing operational efficiency, safety, and data-driven decision-making. Features such as “Find my Asset,” route optimization, and time-in-zone analytics allow businesses to visualize movement patterns and optimize spatial usage.
FiLo and Cardinal are designed for scalability, security, and seamless integration, with user roles ranging from general users to super administrators. The platform supports predictive analytics, machine learning, and pay-per-use models, allowing businesses to grow with their use case needs.
Ultimately, Danalto transforms physical environments into intelligent, measurable spaces.
FiLo™
Danalto’s FiLo™ service is a high resolution (decimeter-scale), Enterprise grade proximity, location, tracking and navigation solution for indoor location. FiLo is deployable in complex enterprise indoor environments, such as multi-room offices, campuses, hospitals, etc... FiLo is designed to be easily deployed with enterprise infrastructure like Wi-Fi Access-Points, to deliver accurate indoor position-location economically.
Deployed as a complete Enterprise solution, danalto FiLo service employs the latest generation of Ultra-Wideband (UWB) silicon for ranging and location and GNSS for geo-location two way ranging; support for partner networking infrastructure (such as Wi-Fi AP vendors) for secure and robust position and location determination; as well as the latest API integrations to the main Cloud platforms (AWS, Google Cloud, Azure) or bespoke platforms. danalto’s FiLo service is packaged as a SaaS, with the Cloud component publicly available through danalto’s Cardinal™ IoT platform, hosted on AWS.
The FiLo indoor location service can be easily and economically deployed as an overlay on enterprise IT infrastructure such as Wi-Fi Access-Point indoor deployments, where FiLo USB dongles augment the Wi-Fi APs with UWB and GNSS for fine-grained indoor accuracy and automated geo-fixing.

FiLo Dongle
The deployed FiLo modules at your enterprise interact with the cloud-hosted danalto Cardinal IoT platform. But Cardinal can also be supplied on a software-only basis to Original Equipment Manufacturers.
FiLo UWB and GNSS Nodes can be deployed as indoor positioning anchors demonstrating FiLo positioning capability. FiLo Anchors work with positioning devices such as Asset-Tracking UWB Tags and consumer Smartphones, to showcase FiLo positioning performance.
FiLo dongles can be inserted in your enterprise Wi-Fi AP USB ports. FiLo supports deployment such as Cisco’s Application Hosting on your enterprise infrastructure. In addition, the FiLo Adopter Pack can include danalto reference-design Cardinal Border Node hardware that acts as target Wi-Fi APs in your evaluation of FiLo service.