Headquarters: France
Region(s) Served: EMEA
SAMEA Innovation is an innovative company in radiocommunications systems and the IoT field, created in 2016, and founded on a strong expertise in wireless communication and electronic design. The company was initially thought of as an entity to provide the tools necessary for the effective development of connected objects: "Picks and shovels for the IoT gold rush".
The development of IoT indeed requires complex and diversified resources, which are frequently focused on data processing software platforms. This overshadows the object itself, and its connectivity performance is often overlooked.
It is on the strength of this observation that SAMEA Innovation was launched with a first design office activity which has made it possible to support many professionals in # B2B on radio integration, by filling in these weaknesses in the development of connected objects.
Thanks to an ever-stronger experience, SAMEA Innovation decided in 2019 to start developing its own range of products, with the main thrusts: improving Wi-Fi connectivity; precision geolocation indoors and outdoors; and finally the improvement of the quality of life with SENSORIIS®.
With growing activity since then, SAMEA Innovation now has a team of 9 people, each of whom brings their skills to offer optimized solutions in terms of performance, connectivity, cost, and size.
SENSORIIS
SENSORIIS® is an-all-in-one environmental sensor, integrating a remote-control actuator (heaters, lights, openings), for the optimization of energy and air quality monitoring in buildings.
The environmental measurements are transmitted to a data server through 4G/5G, LoRa, Sigfox or Bluetooth networks. Multi-protocol communication is fully supported by the built-in antennas to ensure full coverage and use in all regions and countries around the world.

SAM-Connect
SAM24G58xx are a dual band 2.4GHz and 5GHz bi-directional amplifier compliant with IEEE 802.11b/g/a/n/ac WIFI standard.
The booster allows increasing communication distance, speed and is provided with an omni-directional antenna.

LOCIIS
Asset tracker technology with high accuracy everywhere; Localisation outdoor and indoor