NETGEAR Chooses Qorvo's Wireless 802.11ac Amplifier Technology for New Nighthawk® Router

November 17, 2015

The World's Fastest 802.11ac Smart Wi-Fi Router

GREENSBORO, NC and HILLSBORO, OR – November 17, 2015 – Qorvo® (Nasdaq: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications, announced that NETGEAR®, a global supplier of consumer Wi-Fi routers, has selected Qorvo's RFPA5542 5GHz wireless local area network (WLAN) power amplifier (PA) module for its Nighthawk® X8 AC5300 Smart WiFi Router (R8500).

"The Nighthawk router series provides the best-in-class performance to fuel ever-increasing demands for Wi-Fi speed, coverage and throughput," said Sandeep Harpalani, senior director of product marketing, NETGEAR. "Qorvo's high-power, high-efficiency Wi-Fi amplifier technology used on Nighthawk X8 helps us deliver the world's fastest wireless home network connection, giving our customers unparalleled wireless coverage and performance for the growing number of connected devices in the home."

The Nighthawk X8 Tri-Band Quad-Stream 802.11ac WiFi Router, with Qorvo's RFPA5542 PA, enhances throughput for every device in the home. The Tri-Band technology maximizes the number of multiple input, multiple output (MIMO) streams, allows for high-definition video streaming, online gaming and roaming with a strong signal anywhere in the home. The Nighthawk enables 8 streams of 5GHz Wi-Fi powered by the RFPA5542 providing extended range and maximum throughput for a myriad of home devices.

James Klein, Qorvo's president of Infrastructure and Defense products, said, "Qorvo is proud to provide global networking leader NETGEAR with the market's best 802.11ac Wi-Fi amplifier technology, optimized for the highest data rates supported by the 11ac standard. Our industry-leading technology delivers unparalleled speed and simultaneous coverage for multiple devices paving the way for the Internet of Things (IoT) within the home."

The RFPA5542 PA is the device of choice on the latest 4x4 and Tri-Band chipset solutions in the market today, due to its ability to provide market-leading power consumption and power-added efficiency (PAE) at 17 percent for 802.11ac speeds, and over 20 percent for 802.11n speeds. Moreover, the integrated module eliminates the need for external components, greatly reducing system design complexity, layout area, bill of materials and manufacturing cost for the customer application. The RFPA5542 PA is available in 4mm x 4mm standard QFN packaging.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 7,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

About NETGEAR Inc.

NETGEAR (NASDAQ: NTGR) is a global networking company that delivers innovative products to consumers, businesses and service providers. The Company's products are built on a variety of proven technologies such as wireless, Ethernet and powerline, with a focus on reliability and ease-of-use. The product line consists of wired and wireless devices that enable networking, broadband access and network connectivity. These products are available in multiple configurations to address the needs of the end-users in each geographic region in which the Company's products are sold. NETGEAR products are sold in approximately 39,000 retail locations around the globe, and through approximately 31,000 value-added resellers. The company's headquarters are in San Jose, Calif., with additional offices in approximately 25 countries. More information is available at http://investor.netgear.com.

©2015 NETGEAR, Inc. NETGEAR, and Nighthawk are trademarks and/or registered trademarks of NETGEAR, Inc. and/or its affiliates in the United States and/or other countries. Other brand and product names are for identification purposes only and may be trademarks or registered trademarks of their respective holder(s). The information contained herein is subject to change without notice. NETGEAR shall not be liable for technical or editorial errors or omissions contained herein. All rights reserved.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
NETGEAR Chooses Qorvo's Wireless 802.11ac Amplifier Technology for New Nighthawk® Router

November 17, 2015

The World's Fastest 802.11ac Smart Wi-Fi Router

GREENSBORO, NC and HILLSBORO, OR – November 17, 2015 – Qorvo® (Nasdaq: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications, announced that NETGEAR®, a global supplier of consumer Wi-Fi routers, has selected Qorvo's RFPA5542 5GHz wireless local area network (WLAN) power amplifier (PA) module for its Nighthawk® X8 AC5300 Smart WiFi Router (R8500).

"The Nighthawk router series provides the best-in-class performance to fuel ever-increasing demands for Wi-Fi speed, coverage and throughput," said Sandeep Harpalani, senior director of product marketing, NETGEAR. "Qorvo's high-power, high-efficiency Wi-Fi amplifier technology used on Nighthawk X8 helps us deliver the world's fastest wireless home network connection, giving our customers unparalleled wireless coverage and performance for the growing number of connected devices in the home."

The Nighthawk X8 Tri-Band Quad-Stream 802.11ac WiFi Router, with Qorvo's RFPA5542 PA, enhances throughput for every device in the home. The Tri-Band technology maximizes the number of multiple input, multiple output (MIMO) streams, allows for high-definition video streaming, online gaming and roaming with a strong signal anywhere in the home. The Nighthawk enables 8 streams of 5GHz Wi-Fi powered by the RFPA5542 providing extended range and maximum throughput for a myriad of home devices.

James Klein, Qorvo's president of Infrastructure and Defense products, said, "Qorvo is proud to provide global networking leader NETGEAR with the market's best 802.11ac Wi-Fi amplifier technology, optimized for the highest data rates supported by the 11ac standard. Our industry-leading technology delivers unparalleled speed and simultaneous coverage for multiple devices paving the way for the Internet of Things (IoT) within the home."

The RFPA5542 PA is the device of choice on the latest 4x4 and Tri-Band chipset solutions in the market today, due to its ability to provide market-leading power consumption and power-added efficiency (PAE) at 17 percent for 802.11ac speeds, and over 20 percent for 802.11n speeds. Moreover, the integrated module eliminates the need for external components, greatly reducing system design complexity, layout area, bill of materials and manufacturing cost for the customer application. The RFPA5542 PA is available in 4mm x 4mm standard QFN packaging.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 7,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

About NETGEAR Inc.

NETGEAR (NASDAQ: NTGR) is a global networking company that delivers innovative products to consumers, businesses and service providers. The Company's products are built on a variety of proven technologies such as wireless, Ethernet and powerline, with a focus on reliability and ease-of-use. The product line consists of wired and wireless devices that enable networking, broadband access and network connectivity. These products are available in multiple configurations to address the needs of the end-users in each geographic region in which the Company's products are sold. NETGEAR products are sold in approximately 39,000 retail locations around the globe, and through approximately 31,000 value-added resellers. The company's headquarters are in San Jose, Calif., with additional offices in approximately 25 countries. More information is available at http://investor.netgear.com.

©2015 NETGEAR, Inc. NETGEAR, and Nighthawk are trademarks and/or registered trademarks of NETGEAR, Inc. and/or its affiliates in the United States and/or other countries. Other brand and product names are for identification purposes only and may be trademarks or registered trademarks of their respective holder(s). The information contained herein is subject to change without notice. NETGEAR shall not be liable for technical or editorial errors or omissions contained herein. All rights reserved.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.