DALLAS, TX – May 23, 2018 – The ACT88320 PMIC is an integrated ActivePMU™ power management unit that is optimized for space constrained applications like Solid State Drives (SSD), Video Doorbell, Action Camera and other video processing applications. It includes 3 fully integrated DC/DC step down converters and 2 low-dropout regulators (LDOs). The ACT88320 also includes a high-power load switch controller, enabling Over Voltage protection up to 20V, Over Current Protection and Inrush Current control.
Active-Semi's Field Programmable Power Management ICs (PMICs) enable the greatest power density for customers with space constrained application requirements. With the ACT88320 Active-Semi adds to their growing family of PMICs providing benchmark performance in the smallest footprint possible while providing unparalleled flexibility by utilizing patented Programmable Analog features.
Most characteristics and features of the Programmable Analog ICs can be individually set, modified, and controlled via on-board non-volatile memory settings. The programmable voltage levels, currents, slew-rates, push-button control, and other options are field programmable via I2C, set via GPIOs, or by factory preset.
The ACT88320 PMIC is available in a 4 x 4 mm 32 pin QFN package.
"With its high level of integration, flexibility and programmability, the ACT88320 increases system reliability and reduces overall size and power consumption in multiple target applications. Utilizing Active-Semi's software GUI and evaluation board, our customers are able to reduce development effort and time to market." says Bernd Krafthoefer, Marketing Director of Active-Semi Inc.
To find more information please visit:
www.qorvo.com/products/p/ACT88320
Please visit www.qorvo.com/how-to-buy for additional contact and purchasing information.
About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.
Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries. All other trademarks are the property of their respective owners.
|
Media Contact: |