March 1, 2022 | Boston, MA: Anokiwave, Inc., the leader in highly integrated, cost-effective silicon-based IC solutions for the millimeter-wave (mmW) and active antenna markets has introduced both its 4th generation of high efficiency multi-band silicon beamformer ICs as well as industry’s first single-chip dual channel IF up/down converter with fully integrated LO synthesizer. This new Gen-4 IC family enables greener, lower cost, and smaller form factor mmW 5G radios, for every 3GPP FR2 band.
Anokiwave recently announced the release of its Gen-4 mmW silicon ICs that offers a unique combination of industry’s highest linear power and output efficiency devices. ICs in this family include the 24 to 30 GHz AWMF-0221, a quad channel, dual polarization beamforming IC, the AWMF-0210, a wideband IF up/down converter IC, and the AWMF-0224, a dual channel IF transceiver IC. The IC family provides a complete mmW to IF signal chain solution for n257, n258, and n261 frequency bands (24 – 30 GHz) while meeting all 3GPP specs, supporting high signal and 5G NR modulation bandwidths as well as 802.11ac/802.11ax waveforms for private wireless networks.
The new ICs offer a wide range of benefits to the 5G OEMs and network operators, such as:
“Anokiwave is dedicated to enabling the success of OEMs in the mmW 5G market with key innovations that provide critical market solutions,” said Robert S Donahue, Anokiwave CEO. “We understand that an effective mmW 5G network requires the right combination of innovation and cost effectiveness. That’s why we will continue to be a reliable partner in delivering innovative and visionary advanced 5G technologies that meet the industry’s growing demands, providing integrated, lower cost solutions with increased performance capabilities.”
Anokiwave is expected to release devices for additional mmW frequency bands covering as high as 48 GHz later this year.