Anokiwave, NXP Semiconductors, YTTEK, and Semicomm demonstrated an end-to-end FR2 Open RAN solution during a recent seminar in Taipei, Taiwan, with overwhelming attendance and response.


    Download full size image

    January 25, 2022 | Boston, MA: Anokiwave [Now Qorvo], NXP, YTTEK, and Semicomm together demonstrated a complete 5G Radio Unit (RU) from baseband to millimeter-wave (mmW) using the Open RAN architecture at a joint seminar recently held in Taiwan. This new platform provides an end-to-end solution for OEMs, ODMs, and operators to develop Open RAN compatible mmW 5G radio units and bring those to market starting as soon as 2022. The partnered companies worked together to build a solution with measured performance using a FR2 5G NR waveform, highlighting the benefits of a true Open RAN partnership between industry players. At this joint seminar and demo, the companies also provided their unique industry perspectives and the latest product information supporting the new solution.

    The O-RAN alliance, established by the world’s major telecom operators, ensures compatibility and interoperability between each 5G radio section, and has gained extensive international support – opening the opportunity for many new manufactures to enter the mmW 5G equipment supply chain.

    “Anokiwave sees an expansion of mmW applications into small cell radio units and into CPE that require an ecosystem that combines the hardware and software necessary for complete solutions,” states Alastair Upton, Anokiwave Chief Strategy Officer. “Working with our partners, we have created a complete plug and play FR2 development platform within the Open RAN architecture that addresses multiple 5G use cases, demonstrating the feasibility of commercial viability and serving as an initial customer reference design.”

    During the seminar, a unique solution developed by YTTEK based on Anokiwave’s mmW beamformer ICs and integrated up/down converter ICs along with NXP’s LA1200 processor was demonstrated. The solution provides an excellent baseline reference design for OEMs to use for their product development.

    “Anokiwave has been a trusted supplier of mmW solutions from the dawn of 5G. The announcement of our next generation of Beamformer ICs at this Seminar further advances our support of the Open RAN eco-system in the region” states Alan Chang, Anokiwave Director of Asia Pacific Sales.

    With growing demand for high performance mmW 5G radio solutions, the market is looking for true open architectures that leverage the best performance of the RF front ends and digital back end. This partnership between Anokiwave, NXP, and YTTEK, validated with a working solution and measured results, is a true testament to the real Open RAN FR2 system that the three companies have together built and enabled.

    Contact Anokiwave for additional information about the solutions presented at the seminar and our next generation of mmW 5G solutions. Full DIGITIMES coverage of the seminar can be found here.