The Quiet Convergence of Power and RF
There was a time when power engineers and RF engineers occupied different ends of the hallway.
The RF team debated noise figure and linearity as if civilization depended on it. The power team worried about volts, amps and whether something might overheat. They shared a PCB but not always a worldview. If a spur appeared in the spectrum, it was clearly an RF problem. If something got hot, that was clearly a power problem.
Life was simpler then.
Today, those hallway boundaries are dissolving. Modern converters switch fast enough that layout parasitics resemble transmission lines. Gate loops behave like resonant structures. Package inductance stops being an afterthought and starts showing up in the lab as an unexpected oscillation.
And when power management is treated casually, the PCB occasionally rewards you with a full laser-light-and-pyrotechnics show.
The oscilloscope glows with overshoot. The spectrum analyzer fills with harmonics you never budgeted for. That tidy switching node becomes a broadband radiator with impressive range and zero respect for your carefully tuned RF front end. A near-field probe appears, wielded like a fire extinguisher.
The board may not literally ignite, but it can behave as if it is auditioning for a stadium tour.
Fast edges create ringing. Poor loop control creates EMI. A little optimism in the layout can turn a clean design review into spectral damage control. Once the show begins, it is very difficult to argue that power management belongs to someone else’s discipline.
Eventually the smoke clears — metaphorically, one hopes — and the lesson becomes obvious: high frequency is no longer exclusive to the RF team.
At the same time, RF systems have grown far less tolerant of sloppy electrons. AI accelerators, phased array radars, 5G radios and satellite payloads all share a dependency on tightly controlled, dynamically managed power. We celebrate the antenna aperture, beamforming algorithms and heroic PA linearity. But none of those subsystems behave well if the supply rail resembles a suggestion rather than a specification.
Ripple becomes phase noise.
Transients become spectral regrowth.
Impedance becomes destiny.
Consider a modern phased array. Hundreds or thousands of elements must maintain phase coherence while digital control, converters and RF front ends draw from shared power domains. A transient event in one corner of the board can surface elsewhere as jitter, drift or degraded dynamic range. In high order modulation schemes, that becomes degraded EVM. In radar systems, it can mean reduced detection sensitivity.
Efficiency, in this environment, is not merely a thermal metric. It becomes an RF specification.
As systems scale, so does power density. Data centers supporting AI workloads offer a convenient illustration. We speak of “the cloud” as if it floats. In reality, it is racks of silicon pulling tightly regulated current at astonishing speed. Switching frequencies rise to shrink passives and sharpen transient response. Those faster edges introduce coupling paths and parasitics that refuse to be ignored.
The physics is indifferent. Inductance does not care whether it resides in a matching network or a buck converter. A poorly controlled current loop will radiate whether it carries a carrier wave or a switching waveform. Maxwell’s equations remain gloriously impartial.
This is where the quiet revolution in power management becomes compelling. The focus is shifting from delivering power to managing it intelligently. Adaptive control loops respond in real time. Power domains are segmented to isolate sensitive circuits. Integration reduces loop area and parasitic uncertainty. Packaging and layout are treated as electromagnetic structures, not mechanical necessities.
In other words, power design increasingly looks like RF design — just with larger currents and fewer Smith charts.
For microwave engineers, this convergence is both challenge and opportunity. The electromagnetic environment inside modern systems is crowded. High di/dt edges, dense routing and compact integration leave little margin for wishful thinking. Power integrity analysis belongs in the same conversation as S-parameters and stability circles.
The opportunity is equally clear. RF engineers already think in terms of impedance, resonance and coupling. Applying that intuition to power distribution networks and switching loops can elevate overall system performance. When the supply rail is treated as part of the signal chain rather than background infrastructure, the architecture becomes more predictable and more robust.
Power management is no longer the quiet corner of the board that “just has to work.” In high-performance infrastructure, aerospace and defense systems, it is a lever for differentiation. A well-managed power architecture enables higher linearity, lower noise floors and tighter timing margins. It allows RF subsystems to operate closer to their limits without being sabotaged by their own energy source.
We often talk about pushing the boundaries of frequency. Just as important is pushing the boundaries of how precisely we manage the energy that makes those frequencies possible.
The best light show, after all, is the one that never makes it past the layout review.
This article first appeared in Brent's Musings in Microwave Journal.