Qorvo Advances Next-Generation DOCSIS 3.1 Performance

October 8, 2015

Power Doubler Amplifier Offers Industry-leading Power Consumption and Linearity for New Fiber-to-the-Home Services

GREENSBORO, NC and HILLSBORO, OR – Oct 08, 2015 – Qorvo®, Inc. (NASDAQ: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications, today announced the availability of the RFPD3580 power doubler amplifier, offering the lowest power consumption and highest output capability for cable TV (CATV) DOCSIS 3.1 systems.

DOCSIS 3.1 - RFPD3580

Qorvo's RFPD3580 provides high output capability for

45MHz-1.218GHz CATV amplifier systems, excellent

linearity and superior return loss performance with robust

reliability.

Qorvo's RFPD3580 hybrid power doubler amplifier module features advanced gallium nitride on silicon carbide (GaN on SiC) and gallium arsenide (GaAs) process technologies. The RFPD3580 provides high output capability for 45MHz-1.218GHz CATV amplifier systems, excellent linearity and superior return loss performance with robust reliability. Notably, the RFPD3580 operates at an industry-best 18-watt power consumption and is unconditionally stable under all terminations.

Kellie Chong, director of CATV and Broadband Access products at Qorvo, said, "DOCSIS 3.1 increases bandwidth to 1.218GHz, supports higher data rates and more digital content. A new DOCSIS 3.1 Hybrid Fiber Coaxial (HFC) architecture, Fiber Deep (Node+0) is designed to reduce the number of PAs, but puts higher performance demands on the power doubler amplifier. The high performance RFPD3580 power doubler is designed to meet output requirements for this new architecture at the lowest power consumption."

As the leading supplier of CATV GaN solutions with over 2 million units shipped to date, Qorvo is further expanding its portfolio of DOSCIS 3.1 solutions to help cable operators and MSOs optimize available spectrum and increase throughput across their networks to better support increasing subscriber demand for new and improved broadband services.

Qorvo's DOCSIS 3.1 product portfolio includes more than 60 products, including power doubler amplifiers, push-pull amplifiers, pre-driver gain blocks, attenuators, and switches. Qorvo's DOCSIS 3.1 forward path amplifiers operate from 45MHz to 1.2GHz, with very high output (capable of 74dBmV composite power); extremely low distortion levels (lower than 70dBc); and excellent input and output return loss (-20dB typical). Qorvo's reverse path amplifiers operate up to 300MHz with integrated attenuator and power down function. The company's DOCSIS 3.1 solutions employ the latest high-performance process technologies, including GaN high-electron-mobility transistor (HEMT) technology, which delivers superior linearity, output power and reliability needed to equip high-speed cable infrastructure networks.

Qorvo's DOCSIS 3.1 products are packaged in SOT-115J, multi-chip module (MCM), and standard monolithic microwave integrated circuit (MMIC) packaging, including QFN, SOT89, and SOIC. Qorvo's MMIC products include gain amplifiers, low equivalent input noise current (EINC) trans-impedance amplifiers (TIA), attenuators, switches, filters, and complete optical receivers for RF over glass (RFoG) and passive optical network (PON) applications. For more information about Qorvo's line of DOCSIS 3.1 products, download the Qorvo Broadband DOCSIS 3.1 Solutions brochure.

Qorvo will be exhibiting at the SCTE 2015 Cable-Tec Expo in New Orleans, LA, from October 14, 2015, through October 16, 2015.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 6,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.
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
Qorvo Advances Next-Generation DOCSIS 3.1 Performance

October 8, 2015

Power Doubler Amplifier Offers Industry-leading Power Consumption and Linearity for New Fiber-to-the-Home Services

GREENSBORO, NC and HILLSBORO, OR – Oct 08, 2015 – Qorvo®, Inc. (NASDAQ: QRVO), a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications, today announced the availability of the RFPD3580 power doubler amplifier, offering the lowest power consumption and highest output capability for cable TV (CATV) DOCSIS 3.1 systems.

DOCSIS 3.1 - RFPD3580

Qorvo's RFPD3580 provides high output capability for

45MHz-1.218GHz CATV amplifier systems, excellent

linearity and superior return loss performance with robust

reliability.

Qorvo's RFPD3580 hybrid power doubler amplifier module features advanced gallium nitride on silicon carbide (GaN on SiC) and gallium arsenide (GaAs) process technologies. The RFPD3580 provides high output capability for 45MHz-1.218GHz CATV amplifier systems, excellent linearity and superior return loss performance with robust reliability. Notably, the RFPD3580 operates at an industry-best 18-watt power consumption and is unconditionally stable under all terminations.

Kellie Chong, director of CATV and Broadband Access products at Qorvo, said, "DOCSIS 3.1 increases bandwidth to 1.218GHz, supports higher data rates and more digital content. A new DOCSIS 3.1 Hybrid Fiber Coaxial (HFC) architecture, Fiber Deep (Node+0) is designed to reduce the number of PAs, but puts higher performance demands on the power doubler amplifier. The high performance RFPD3580 power doubler is designed to meet output requirements for this new architecture at the lowest power consumption."

As the leading supplier of CATV GaN solutions with over 2 million units shipped to date, Qorvo is further expanding its portfolio of DOSCIS 3.1 solutions to help cable operators and MSOs optimize available spectrum and increase throughput across their networks to better support increasing subscriber demand for new and improved broadband services.

Qorvo's DOCSIS 3.1 product portfolio includes more than 60 products, including power doubler amplifiers, push-pull amplifiers, pre-driver gain blocks, attenuators, and switches. Qorvo's DOCSIS 3.1 forward path amplifiers operate from 45MHz to 1.2GHz, with very high output (capable of 74dBmV composite power); extremely low distortion levels (lower than 70dBc); and excellent input and output return loss (-20dB typical). Qorvo's reverse path amplifiers operate up to 300MHz with integrated attenuator and power down function. The company's DOCSIS 3.1 solutions employ the latest high-performance process technologies, including GaN high-electron-mobility transistor (HEMT) technology, which delivers superior linearity, output power and reliability needed to equip high-speed cable infrastructure networks.

Qorvo's DOCSIS 3.1 products are packaged in SOT-115J, multi-chip module (MCM), and standard monolithic microwave integrated circuit (MMIC) packaging, including QFN, SOT89, and SOIC. Qorvo's MMIC products include gain amplifiers, low equivalent input noise current (EINC) trans-impedance amplifiers (TIA), attenuators, switches, filters, and complete optical receivers for RF over glass (RFoG) and passive optical network (PON) applications. For more information about Qorvo's line of DOCSIS 3.1 products, download the Qorvo Broadband DOCSIS 3.1 Solutions brochure.

Qorvo will be exhibiting at the SCTE 2015 Cable-Tec Expo in New Orleans, LA, from October 14, 2015, through October 16, 2015.

About Qorvo

Qorvo (NASDAQ:QRVO) is a leading provider of core technologies and RF solutions for mobile, infrastructure and aerospace/defense applications. Qorvo was formed following the merger of RFMD and TriQuint, and has more than 6,000 global employees dedicated to delivering solutions for everything that connects the world. Qorvo has the industry's broadest portfolio of products and core technologies; world-class ISO9001-, ISO 14001- and ISO/TS 16949-certified manufacturing facilities; and is a DoD-accredited 'Trusted Source' (Category 1A) for GaAs, GaN and BAW products and services. For the industry's leading core RF solutions, visit www.qorvo.com.

Qorvo Media Contact

Katie Caballero
Marketing Communications Manager
Qorvo Infrastructure and Defense Products
+1-972-994-8546
katie.caballero@qorvo.com

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. Qorvo's business is subject to numerous risks and uncertainties, including variability in operating results, the inability of certain of our customers or suppliers to access their traditional sources of credit, our industry's rapidly changing technology, our dependence on a few large customers for a substantial portion of our revenue, our ability to implement innovative technologies, our ability to bring new products to market and achieve design wins, the efficient and successful operation of our wafer fabrication facilities, assembly facilities and test and tape and reel facilities, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, variability in manufacturing yields, industry overcapacity and current macroeconomic conditions, inaccurate product forecasts and corresponding inventory and manufacturing costs, dependence on third parties and our ability to manage channel partners and customer relationships, our dependence on international sales and operations, our ability to attract and retain skilled personnel and develop leaders, the possibility that future acquisitions may dilute our shareholders' ownership and cause us to incur debt and assume contingent liabilities, fluctuations in the price of our common stock, additional claims of infringement on our intellectual property portfolio, lawsuits and claims relating to our products, security breaches and other similar disruptions compromising our information and exposing us to liability, the impact of stringent environmental regulations, and the impact of the integration of Qorvo. These and other risks and uncertainties, which are described in more detail in Qorvo's 8K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

Stay up to date with us.

Sign up for notification on new products, product/process change notifications (PCNs) and end of life (EOL) alerts.

Sign Up

Qorvo products are at work connecting, protecting and powering the planet. We bring core radio frequency (RF) and power technologies and solutions to automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure and mobile markets.