February 22, 2019 | San Diego, CA: Anokiwave today announced the next product in a new family of second generation 5G Silicon Quad Core ICs that enable 3GPP compliant base stations with the worldwide release of the 28 GHz AWMF-0157 IC. The second-generation IC family is part of Anokiwave’s on-going strategy to enable the commercialization of 5G mmW systems with silicon ICs.
The AWMF-0157 operates at 26.5 – 29.5 GHz, supports 4 radiating elements, and includes gain and phase controls for analog RF beam steering. Anokiwave’s patent-pending IP blocks implemented in silicon technology enable low-cost hybrid beam forming with high energy efficiency and low latency beam steering™.
“As the push to roll out 5G networks by the end of the year is proceeding at full speed, Anokiwave is executing on an aggressive strategy to deliver mmW 5G solutions with industry first ICs at 26 GHz, 28 GHz, and 39 GHz,” states David Corman, Anokiwave Chief Architect. “Today’s announcement of the new family of ICs that enable 3GPP compliance is an essential step that allows network operators to roll out 5G coverage in earnest.”
The AWMF-0157 is a highly integrated silicon IC packaged in a wafer level chip scale package (WLCSP), easily fitting within the typical 5.3 mm lattice spacing at 28 GHz.